Everything
2.9.1 Display/change the memory

The contents of the memory can be displayed and its values can be changed in the Memory panel below.

Select the [View] menu >> [Memory] >> [Memory1 - 4].

The maximum of 4 Memory panels can be opened. Each panel is identified by the names "Memory1", "Memory2", "Memory3" and "Memory4" on the titlebar.

For details on the contents and function in each area, see the section for the Memory panel.

Figure 2.47

Display the Contents of Memory (Memory Panel)

(1): Address area

(2): Memory value area

(3): Character strings area

Remark

You can set the scroll range (as start and end address) of the vertical scroll bar on this panel via the Scroll Range Settings dialog box that is opened by clicking the button from [View] on the toolbar.

 

This section describes the following.

 

2.9.1.1 Specify the display position

2.9.1.2 Change display format of values

2.9.1.3 Modify the memory contents

2.9.1.4 Display/modify the memory contents during program execution

2.9.1.5 Search the memory contents

2.9.1.6 Modify the memory contents in batch (initialize)

2.9.1.7 Save the memory contents