Everything
2.9.3.1 Search for a SFR

A SFR can be searched for.

Specify the SFR name to search with the text box in the search area (case-insensitive). You can either type character strings directly from the key board (up to 512 characters), or select one from the input history via the drop-down list (up to 10 items).

Then, click either one of the following button.

 

Searches up for the SFR name containing the string specified in the text box, and selects the SFR that is found.

 

Searches down for the SFR name containing the string specified in the text box, and selects the SFR that is found.

Remark 1.

The hidden SFR name being classified with a category can be searched (the category is opened and the SFR is selected).

Remark 2.

After typing character strings to search, to press the [Enter] key is the same function as clicking the button, and to press the [Shift] + [Enter] key is the same function as clicking the button.