The following types of CS+ execution functions are provided.
Select any of the following operations according to the purpose of debugging.
See "2.8 Stop Programs (Break)" for details on how to stop the program in execution.
2.7.2.1 Execute after resetting microcontroller (CPU)
2.7.2.2 Execute from the current address
2.7.2.3 Execute after changing PC value
You can automatically overwrite the value of SFR/CPU register with the specified values before starting program execution (see "2.16 Use Hook Function" for details). |