Even when an Intel HEX file (*.hex), Motorola S-record file (*.mot) or binary file (*.bin) is specified to be the subject file to download, it is possible to do source level debugging by downloading symbol information for the load module file from which the subject file was created, along with the subject file that you download.
To do so, follow the steps below on the Download Files dialog box.
When the [Add] button is clicked, a blank list item "-" is displayed in the last line of the [Download file list] area.
Configure each item displayed with the following condition in the [Download file property] area.
|
Specify a load module file from which the Intel HEX file (*.hex), Motorola S-record file (*.mot) or binary file (*.bin) that you want to download was created. Directly enter from the keyboard, or specify with the Select Download File dialog box that is opened by clicking the [...] button that appears at right by selecting this property. |
|||
|
Select whether to generate the information for the Symbol name completion function when downloadingNote. |
|||
|
Generates the information for the symbol name completion function. (i.e. uses the symbol name completion function.) |
|||
|
Does not generate the information for the symbol name completion function. (i.e. does not use the symbol name completion function.) |
|||
When [Yes] is selected, the time taken for downloading and the memory usage on the host machine will increase. We recommend selecting [No] in this item if you do not intend to use the symbol name completion function. |
Enable all the configuration in this dialog box and add the specified load module file (Only the symbol information included in the load module file will be downloaded).