The I/O register values can be edited.
In the [Value] area, click the selected I/O register value again to set it in the Edit mode (Pressing the [Esc] key cancels the edit mode).
Edit the value directly from the keyboard and then press the [Enter] key. The value you've changed is written into the debug tool's target memory.
If a number with fewer digits than the size of the I/O register is entered, the higher-order digits will be padded with zeroes. |
If a number with more digits than the size of the I/O register is entered, the higher-order digits will be masked. |
When "0x41" is entered as the value of I/O register “CRC.CRCDOR” |