This class holds timer information (return value of the debugger.XTime function).
[Type]
class XTimeInfo:
Value = 0
IsCpuClock = False
IsOverFlow = False
|
[Variable]
|
|
|
|
Value
|
This holds the timer measurement.
|
|
IsCpuClock
|
This holds whether this is a CPU clock measurement or not.
True: This is a CPU clock measurement.
False: Otherwise.
|
|
IsOverFlow
|
This holds whether an overflow has occurred or not.
True: An overflow has occurred.
False: An overflow has not occurred.
|
[Detailed description]
- | XTimeInfo is a class, and it is the structure of the return value from the debugger.XTime function. |
[Example of use]
>>>info = debugger.XTime()
9820214200nsec
>>>print info.Value
9820214200
>>>print info.IsCpuClock
False
>>>print info.IsOverFlow
False
>>>
|