This function adds a file to the active project.
[Specification format]
project.File.Add(fileName, category = "")
|
[Argument(s)]
|
|
|
|
fileName
|
Specify the full path of the file to be added to the active project.
When specifying multiple files, specify in the format ["file1", "file2"].
|
|
category
|
Specify the category that the file is added (default: not specified).
When specifying multiple levels, specify in the format ["one", "two"].
|
[Return value]
If a file was added to the active project successfully: True
If there was an error when a file was added to the active project: False
If there was an error when any files were added to the active project when multiple files were specified for fileName: False
[Detailed description]
- | This function adds the file specified in fileName to the active project. |
- | If category is specified, the file is added below that category.
If the specified category does not exist, it is created newly. |
[Example of use]
>>>project.File.Add("C:/project/sample/src/test.c", "test")
True
>>>project.File.Add(["C:/project/sample/src/test1.c", "C:/project/sample/src/test2.c"], ["test", "src"])
True
|