This function runs a build of a specified file.
[Specification format]
build.File(fileName, rebuild = False, waitBuild = True)
|
[Argument(s)]
|
|
|
|
fileName
|
Specify a file to run a build.
|
|
rebuild
|
Specify whether to run a rebuild of a specified file.
True: Run a rebuild of a specified file.
False: Run a build of a specified file (default).
|
|
waitBuild
|
Specify whether to wait until completing a build.
True: Wait until completing a build (default).
False: Return a prompt without waiting to complete a build.
|
[Return value]
- | When waitBuild is set to "True" |
If a build was completed successfully: True
If there was an error when running a build: False
- | When waitBuild is set to "False" |
If a build successfully started execution: True
If a build failed to start execution: False
[Detailed description]
- | This function runs a build of a file specified by fileName. |
- | If rebuild is set to "True", then a rebuild of a specified file is run. |
- | If waitBuild is set to "False", then a prompt is returned without waiting to complete a build. |
[Example of use]
>>>build.File("C:/test/test.c")
True
>>>
|