This property switches the write-time verification setting. [Except simulator]
[Specification format]
debugger.Memory.NoVerify = noverify
|
[Setting(s)]
|
|
|
|
noverify
|
Set whether to verify during writes.
True: Verify during writes.
False: Do not verify during writes.
|
[Reference]
Set value
Caution | If a PM+ workspace is converted to a CS+ project, then there will be no debugging tool in the main project. For this reason, "None" will be returned if the main project is the active project. |
[Detailed description]
- | This property switches the write-time verification setting. |
[Example of use]
>>>print debugger.Memory.NoVerify
False
>>>debugger. Memory.NoVerify = True
>>>print debugger. Memory.NoVerify
True
>>>
|