Add a load module file to the debug-dedicated project as the download file to debug.
To perform source level debugging (step execution in source level units, etc.), a load module file with the symbol information must be added to the debug-dedicated project. |
The specified load module file is reflected automatically on the [Download File Settings] tab in the Property panel of the debugging tool. |
A load module file can be added by the following methods.
Drag a load module file from Explorer or the like, and drop it onto the Download files node on the project tree.
![](ProjectOperation_Eng-564.gif)
Select the Download files node on the project tree, and then select [Add] >> [Add New File...] from the context menu. The Add File dialog box will open.
![](ProjectOperation_Eng-565.gif)
In the dialog box, specify the file name to be created newly and the location in which it is created, and then click the [OK] button.
The project tree after adding the load module file will look like the one below.
![](ProjectOperation_Eng-566.gif)