Use this category to configure general settings relating to the external text editor.
![](ProjectOperation_Eng-369.gif)
The following items are explained here.
Either type in the name of the executable file (including absolute path) for the external text editor directly via the keyboard (up to 259 characters), or click the [Browse...] button, and in the Select External Text Editor dialog box, specify the name of the executable file.
This item is only enabled if the [Use external text editor] check box is selected.
Specify the startup options (without the line number) for the external text editor (up to 256 characters).
This item is only enabled if the [Use external text editor] check box is selected.
The following placeholders can be specified by the
button.
If you wish to specify more than one option, separate them by spaces.
Specify the startup options (with the line number) for the external text editor (up to 256 characters).
This item is only enabled if the [Use external text editor] check box is selected.
The following placeholders can be specified by the
button.
If you wish to specify more than one option, separate them by spaces.
This item is only enabled if the [Use external text editor] check box is selected.
Suppresses starting an external text editor and opens the file to display in the Editor panel during debugging (default). |
|
Restores all settings on this dialog box to their default values. Note, however, that newly added items in the [General - External Tools] category will not be removed. |
|