Everything
 

[Subproject] tab


This tab shows the detailed information on subproject categorized by the following and the configuration can be changed.

 

(1) [File]

(2) [License]

(3) [Notes]

[Description of each category]

(1)

[File]

The detailed information on files is displayed.

File name

Displays the file name of the file to save the information on the subproject.

Default

Name of the subproject file

How to change

Changes not allowed

Relative path

Displays the relative path of the subproject file to which subproject information is saved, from the location of the main project.

This property is shown only when the subproject is selected in Project Tree panel. Note that if the relative path does not exist (such as the case that the main project and subproject are in the different drive), it is not displayed.

Default

Relative path from the main project

How to change

Changes not allowed

Absolute path

Displays the absolute path of the subproject file to save the information on them.

Default

Absolute name of subprojects.

How to change

Changes not allowed

Save with absolute path

Select whether to save the subproject information to a subproject file using the absolute path.

Default

No

How to change

Select a value from the drop-down list.

Restriction

Yes

Saves the file using the absolute path.

No

Saves the file using the relative path.

(2)

[License]

The detailed information on a license is displayed and their configuration can be changed.

Use standard edition for floating license

Select whether to use only a floating license for the standard edition.

Default

Yes

How to change

Select a value from the drop-down list.

Restriction

Yes

Uses a floating license for the standard edition.

No

Uses a floating license for editions other than the standard edition.

Standard edition for floating license is currently in use

Displays if a floating license for the standard edition is used.

Default

Yes

How to change

Changes not allowed

(3)

[Notes]

The detailed information on records is displayed and their configuration can be changed.

Memo

Add memos to subprojects.

Memo is added one item in one line.

The added memos are displayed as subproperty.

Default

Memo [Number of items]

How to change

Edit by the Text Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can use a text box directly enter the text.

Restriction

Up to 256 characters

Up to 256 characters are allowed.