The display format of the address area/memory value area/character strings area can be changed using buttons
|
Shows the following buttons that change the form in which memory values are displayed. |
||
|
Shows the following buttons that change the form in which size of memory values are displayed. |
||
|
Displays memory values in 16-bit width. Values are converted depending on the endian of the target memory area. |
||
|
Displays memory values in 32-bit width. Values are converted depending on the endian of the target memory area. |
||
|
Displays memory values in 64-bit width. Values are converted depending on the endian of the target memory area. |
||
|
Shows the following buttons that change the encoding in which character strings are displayed. |
||
|
Displays character strings as a half-precision floating-point value. |
||
|
Displays character strings as a single-precision floating-point valueNote. |
||
|
Displays character strings as a double-precision floating-point value. |
||
|
Displays character strings as a complex number of single-precision floating-point. |
||
|
Displays character strings as a complex number of double-precision floating-point. |
||
|
Displays character strings as an imaginary number of single-precision floating-point. |
||
|
Displays character strings as an imaginary number of double-precision floating-point. |
||
|
Opens the Scroll Range Settings dialog box to set the scroll range. |
||
|
Opens the Column Number Settings dialog box to set the number of view columns in the memory value area. |
||
|
Opens the Address Offset Settings dialog box to set an offset value for addresses displayed in the address area. |
||
For details on the display of a floating-point value, see the section for the Memory panel. |
Hexadecimal
Signed Decimal
Unsigned Decimal
Octal
Binary
4 Bits
1 Byte
2 Bytes
4 Bytes
8 Bytes
ASCII
Shift_JIS
EUC-JP
UTF-8
UTF-16
Half-Precision Float
Float
Double
Float Complex
Double Complex
Float Imaginary
Double Imaginary
Settings Scroll Range...