This property is for setting or referring to the endian of data. It is a common option for the build tool for the active project. [CC-RX]
|
Handles double type and long double type as single-precision floating-point type (4 bytes). |
||
|
Handles double type and long double type as double-precision floating-point type (8 bytes). |
||
This property is for setting or referring to the endian of data. It is a common option for the build tool for the active project. |