Everything
1.2 Features

The features of the analysis tool are shown below.

 

-

Displaying function information

The following information about functions is displayed:
Static analysis information (e.g. function name, file name, attribute, return type, reference count, etc.) and Dynamic analysis information (e.g. execution count, execution time, code coverage, etc.).

 

-

Displaying variable information

The following information about variables is displayed:
Static analysis information (e.g. variable name, file name, attribute, type, reference count, etc.) and Dynamic analysis information (e.g. read count, write count, data coverage, etc.).

 

-

Displaying the call graph

A tree-structured chart (call graph) indicating calling relationships between functions in the program is displayed.

 

-

Displaying class information/function information/variable information

The class information [CC-RX], function information and variable information in the program are displayed in a tree structure.

 

-

Linked operation with debug tool

The following operations can be performed on the debug tool from the various panels of the analysis tool.

-

Jump to the location where the specified function or variable is defined:
Function List panel/Variable List panel/Call Graph panel/Class/Member panel

-

Set a break event at the specified function or variable:
Function List panel/Variable List panel

-

Register a watch expression for the specified variable:
Variable List panel

 

-

View list of locations referencing function/variable

You can find and display a list of locations referencing a function/variable.

 

-

Graph analysis information

-

A line chart indicating changes in values of variables or of data collected for Smart Analog [E1/E2/E2 Lite/E20/COM Port[RL78]] is displayed.

 

-

A pie chart indicating function execution time ratios is displayed.