This tab shows the detailed information on the link phase categorized by the following and the configuration can be changed.
For details on compiler driver options, refer to "MULTI: Building Applications for Embedded V850 and RH850" released by Green Hills Software, LLC. Please do not contact Green Hills Software, LLC with any inquiries about the CCRH850 build-tool plugin of CS+.  | 
This tab is displayed only when the current project has been created with [Empty Application(GHS CCRH850)] or [Library(GHS CCRH850)] selected as the project type.  | 
[Description of each category]
The detailed information on debug information is displayed and the configuration can be changed.
The detailed information on output files is displayed and the configuration can be changed.
The detailed information on the library is displayed and the configuration can be changed.
The detailed information on hex output is displayed and the configuration can be changed.
The detailed information on the list is displayed and the configuration can be changed.
Other detailed information on linking is displayed and the configuration can be changed.