|
R_ATUIV_Timerknm_Get_InputCapturex
|
Reads the input capture register of the timer.
[Syntax]
void R_ATUIV_Timerknm_Get_InputCapturex ( uint32_t * value );
|
Remark | k is the timer kind, n is the unit number, m is the channel number. |
[Argument(s)]
|
|
|
|
|
|
uint32_t * value;
|
Pointer to area in which to store the results of input capture register
|
[Return value]
None.