| 
 R_SCI3m_Multiprocessor_Receive 
 | 
Starts SCI3 data reception by multiprocessor mode.
Remark 1.  | This API function performs byte-level SCI3 reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.  | 
 
Remark 2.  | Starts after this API function is called, and R_SCI3m_Start is then challed.  | 
 
[Syntax]
MD_STATUS R_SCI3m_Multiprocessor_Receive( uint8_t * rx_buf, uint16_t rx_num, uint8_t rx_id); 
 | 
 
Remark  | m is the channel number.  | 
 
[Argument(s)]
| 
 | 
 | 
 | 
| 
 | 
uint8_t * const rx_buf; 
 | 
 
Pointer to a buffer storing the received data 
 | 
| 
 | 
uint16_t rx_num; 
 | 
 
Total amount of data to receive 
 | 
| 
 | 
uint8_t rx_id; 
 | 
 
Reception id 
 | 
 
[Return value]
| 
 | 
 | 
| 
 
MD_OK 
 | 
 
Normal completion 
 | 
| 
 
MD_ARGERROR 
 | 
 
Invalid argument specification 
 |