Sets the operation mode of A/D converter.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_adc.h”
MD_STATUS R_ADC_Set_TestChannel ( test_channel_t channel );
[Argument(s)]
| I/O | Argument | Description | 
| I | test_channel_t channel; | Operation mode of A/D converter ADNORMALINPUT: Normal mode (Normal A/D conver- sion) ADNORMALINPUT: Test mode (AVREFM input) ADNORMALINPUT: Test mode (AVREFP input) | 
[Return value]
| Macro | Description | 
| MD_OK | Normal completion | 
| MD_ARGERROR | Invalid argument specification |