Changes the CPU clock/peripheral hardware clock.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_cgc.h”
MD_STATUS R_CGC_Set_ClockMode ( clock_mode_t mode );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
clock_mode_t mode; |
Clock generator type HIOCLK : High-speed onchip oscillator SYSX1CLK : X1 clock SYSEXTCLK : External main system clock SUBXT1CLK : XT1 clock SUBEXTCLK : External subsystem clock |
[Return value]
|
Macro |
Description |
|
MD_OK |
Normal completion |
|
MD_ERROR1 |
Exit with error (abend) |
|
MD_ERROR2 |
Exit with error (abend) |
|
MD_ERROR3 |
Exit with error (abend) |
|
MD_ERROR4 |
Exit with error (abend) |
|
MD_ARGERROR |
Invalid argument specification |