Performs processing in response to detection of parity error (ACK error).
[Syntax]
#include “r_cg_macrodriver.h”
static void r_iicmn_callback_master_error ( MD_STATUS flag );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| O | MD_STATUS flag; | Cause of communication error MD_NACK: Acknowledge not detected | 
[Argument(s)]
None.
[Return value]
None.