R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Stop
 
Ends forced output stop function 1 for 
timer output TKBOn0.
 
[Syntax]
void   
R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Stop ( void 
);
 
Remark         
m is the unit number, and n is the channel number.
 
[Argument(s)]
None.
 
[Return 
value]
None.