Usage example (Output compare function)
Perform toggle operation at fixed intervals and output a suquare wave with a duty factor of 50%.
[Waveform example]

[GUI setting example]
| 
       Timer  | 
    
       Used  | |||
| 
       TMRD0  | 
    
       Used  | |||
| 
       Output compare function  | 
    
       Used  | |||
| 
       Count source setting  | 
    
       Internal clock  | |||
| 
       Internal clock setting  | 
    
       fIH  | |||
| 
       Counter operation  | 
    
       Count continues at TRDGRA0 comparematch  | |||
| 
       Counter clear  | 
    
       Clear by TRDGRA0 compare match  | |||
| 
       Regiaster function setting(TRDGRC0)  | 
    
       General register  | |||
| 
       Regiaster function setting (TRDGRD0)  | 
    
       General register  | |||
| 
       Compare value setting TRDGRA0  | 
    
       100(μs)(Actual value:100)  | |||
| 
       Output setting TRDIOA0 pin  | 
    
       Initial output “L” Compare match Toggle output  | |||
| 
       Enable TRDGRA0 compare match interrupt  | 
    
       Used  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start TMRD0 counter */
R_TMR_RD0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}