Usage example (PWMmode)
Output PWM function with specified cycle and duty.
[Waveform example]

[GUI setting example]
| 
       TimerRG  | 
    
       Used  | |||
| 
       TMRG  | 
    
       Used  | |||
| 
       Functions  | 
    
       PWM mode  | |||
| 
       Count source setting  | 
    
       Internal clock  | |||
| 
       Internal clock setting  | 
    
       Auto  | |||
| 
       Counter clear  | 
    
       Clear by TRGGRA compare match  | |||
| 
       Register function setting (TRGGRC)  | 
    
       General register  | |||
| 
       Register function setting (TRGGRD)  | 
    
       General register  | |||
| 
       Cycle  | 
    
       100μs (Actual value:100)  | |||
| 
       Duty  | 
    
       50(%) (Actual value:50)  | |||
| 
       Enable TRGGRA compare match interrupt  | 
    
       Used  | |||
| 
       Enable TRGGRB compare match interrupt  | 
    
       Unused  | |||
| 
       Enable TRG overflowinterrup  | 
    
       Unused  | |||
| 
       INTTRG priority  | 
    
       Low/ level3 (low priority level)  | |||
[API setting example]
r_cg_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start the TMRG module operation */
R_TMRG0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}