Starts RIIC slave reception.
Remark 1. This API function performs byte-level RIIC slave reception the number of times specified by the argument rx_num and stores the data in the buffer specified by the argument rx_buf.
Remark 2. When performing a RIIC slave reception, R_RIICn_Start must be called before this API function is called.
[Syntax]
#include "r_cg_macrodriver.h"
MD_STATUS R_RIICn_Slave_Receive ( uint8_t * const rx_buf, uint16_t rx_num );
Remark n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
uint8_t * const rx_buf; |
Pointer to a buffer to store the reception data |
|
I |
uint16_t rx_num; |
Total amount of data to receive |
[Return value]
|
Macro |
Description |
|
MD_OK |
Normal completion |