This option specifies the size of the data record to be output.
[Specification format]
- | Interpretation when omitted |
Various data records are output according to each address.
[Detailed description]
- | This option outputs data with data record record regardless of the address range. |
- | The items that can be specified as record are shown below. |
|
H16
|
HEX record
|
|
H20
|
Expanded HEX record
|
|
H32
|
32-bit HEX record
|
|
S1
|
S1 record
|
|
S2
|
S2 record
|
|
S3
|
S3 record
|
- | If there is an address that is larger than the specified data record, the appropriate data record is selected for the address. |
[Example of use]
- | To output 32-bit HEX record regardless of the address range: |
>rlink a.obj b.obj -record=H32 -form=hexadecimal -output=c.hex
|
[Remark]
- | If the -form={hexadecimal|stype} option is not specified, this option will be invalid. |
- | An error will occur if the -record={S1|S2|S3} option is specified when the -form=hexadecimal option is specified, or if the -record={H16|H20|H32} option is specified when the -form=stype option is specified. |