Classification
Option
Description
Input Options
-Input
Specifies relocatable files.
-library
Specifies library files.
-binary
Specifies binary files.
-define
Specifies symbol definitions.
-entry
Specifies an entry symbol or entry address.
-noprelink
Selects non-initiation of the prelinker.
-allow_duplicate_module_name [V3.02.00 or later]
This option allows multiple same module names to be specified.
Output Options
-form
Selects the output file format.
-debug
Debugging information is output to load module files.
-sdebug
Debugging information is output to the .dbg file.
-nodebug
Debugging information is not output.
-record
Selects the record size.
-end_record [V2.07.00 or later]
This option specifies the end record.
-rom
Specifies the section mapping from ROM to RAM.
-output
Specifies the names of files to be output.
-map
Outputs an external symbol-allocation information file.
-space
Data are output to fill unused ranges of memory.
-message
Information-level messages are output.
-nomessage
The output of messages is disabled.
-msg_unused
Messages are output to indicate the presence of externally defined symbols to which there is no reference.
-byte_count
Specifies the number of bytes in a data record.
-fix_record_length_and_alignment [V2.08.00 or later]
Fixes the format of data records to be output.
-crc
Specifies the format for output of the CRC code.
-padding
Padding data are included at the end of each section.
-vectn
Assigns an address to the specified vector number in the variable vector table (for the RX Family and M16C Family).
-vect
Assigns an address to an unused area in the variable vector table (for the RX Family and M16C Family).
-split_vect [V3.00.00 or later]
Generates split vector table sections.
-jump_entries_for_pic
Outputs a jump table file (for the PIC function of the RX Family).
-cfi [Professional Edition only] [V2.08.00 or later]
Generates the function list for use in detecting illegal indirect function calls.
-cfi_add_func [V2.08.00 or later]
Specifies the symbol or address of a function to be added to the function list for use in detecting illegal indirect function calls.
-cfi_ignore_module [V2.08.00 or later]
Specifies modules which are to be exempted from checking against the function list for use in detecting illegal indirect function calls.
-create_unfilled_area
[To be supported by V2.03 and later versions]
Makes spaces created by .OFFSET unfilled.
List Options
-list
A linkage list file is output.
-show
Selects the contents to be output in the linkage list file.
Optimize Options
-optimize
Selects the items to be optimized at linkage.
-nooptimize
Selects no optimization at linkage.
-samesize
Specifies the minimum size for unification of the same codes.
-symbol_forbid
Specifies symbols for which unreferenced symbol deletion is disabled.
-samecode_forbid
Specifies symbols for which same code unification is disabled.
-section_forbid
Specifies a section where optimization is disabled.
-absolute_forbid
Specifies an address range where optimization is disabled.
Section Options
-start
Specifies a section start address.
-fsymbol
Specifies the section where an external defined symbol will be placed in the output file.
-aligned_section
Specifies the section alignment value as 16 bytes.
Verify Options
-cpu
Checks addresses for consistency.
-contiguous_section
Specifies sections that will not be divided.
Other Options
-s9
Selects the output of an s9 record at the end of the file.
-stack
Selects the output of a stack information file.
-compress
Debugging information are compressed.
-nocompress
Debugging information are not compressed.
-memory
Selects the amount of memory to be used in linkage.
-rename
Specifies symbol names and section names to be modified.
-lib_rename [V3.01.00 or later]
Changes the name of a symbol or section that was input from a library.
-delete
Specifies symbol names and module names to be deleted.
-replace
Specifies library modules to be replaced.
-extract
Specifies modules to be extracted from library files.
-strip
Debugging information is deleted from absolute files and library files.
-change_message
Specifies changes to the levels of messages (information, warning, and error).
-hide
Name information on local symbols is deleted.
-total_size
The total sizes of sections after linkage are sent to standard output.
-verbose [V3.03.00 or later]
This option displays detailed information in the standard error output.
Subcommand File Option
-subcommand
Specifies a file from which to include command options.
Options Other Than Above
-logo
Selects the output of copyright information.
-nologo
Selects the non-output of copyright information.
-end
Selects the execution of option strings specified before END.
-exit
Specifies the end of option specification.