By selecting [Connect to Debug Tool] from the [Debug] menu, CS+ starts communicating with the debug tool selected in the active project.
After succeeding in the connection to the debug tool, the Statusbar of the Main window changes as follows:
For details on each item displayed on the Statusbar, see the section of the Main window.
If the version of compiler being used is not supported by CS+, [Connect to Debug Tool] will be disabled. |
When the |
button on the
button on this toolbar is clicked, the project is built automatically, and then the built file is downloaded after connecting to the debug tool.