2.19.4.2  
Edit access-related events
 
The address condition, data condition and pass count condition [Simulator] for access-related events you have set can be edited.
Perform this operation in the Detail dialog box (for access events) that is opened by selecting [Edit Condition...] from the context menu after moving the caret to an access-related eventNote you want to edit on the Events panel.
Note  | An access-related event refers to any one of the following events in the Events panel.  | 
 
-  | Hardware Break event (access type)  | 
 
-  | Access-related event as start and end condition in detailed information on Trace event  | 
 
-  | Access-related event in detailed information on Point Trace event  | 
 
-  | Access-related event as start and end condition in detailed information on Performance Measurement event  | 
 
For the access-related events that were set according to the descriptions in 2.11.5.1  Set a break event (access type), 2.14.3.1  Set a Trace event, 2.14.4.1  Set a Point Trace event, and 2.16.1.1  Set a Performance Measurement event the initial values of the address, data, and pass count conditions are listed below.
Table 2.25  | Initial Values of Address Conditions  | 
 
| 
 | 
 | 
| 
 | 
 | 
| 
 
Compare condition 
 | 
 
[Full-spec emulator][E1][E20] 
RH850G3M, RH850G3K, RH850G3MH, RH850G3KH: 
 Specified address (==) 
RH850G4MH: 
 When a value for comparison has been specified: 
  Inside the range (<=Addresses<=) 
 When a value for comparison has not been specified: 
  Specified address (==) 
GTM: 
 Inside the range (<=Addresses<=) 
[Simulator] 
 Specified address (==) 
 | 
 
[Full-spec emulator][E1][E20] 
 Inside the range (<=Addresses<=) 
[Simulator] 
 Specified address (==) 
 | 
| 
 
Address 
 | 
 
Address at the time of setting the event 
 | 
| 
 
Start address 
 | 
 
Address at the time of setting the event 
 | 
| 
 
End address 
 | 
 
Address at the time of setting the event 
 | 
| 
 
Use the address mask 
 | 
 
No 
 | 
| 
 
Mask value 
 | 
 
0xFFFFFFFF 
 | 
 
Table 2.26  | Initial Values of Data Conditions  | 
 
| 
 
Item 
 | 
 
Initial Value 
 | 
| 
 
Access type 
 | 
 
Access type at the time of setting the event 
 | 
| 
 
Access size 
 | 
 
Variable or I/O register size at the time of setting the event 
 | 
| 
 
Compare condition 
 | 
 
When a value for comparison has been specified : Specified value (==) 
When a value for comparison has not been specified : No conditions 
 | 
| 
 
Data 
 | 
 
Data at the time of setting the event 
 | 
| 
 
Lower data 
 | 
 
Data at the time of setting the event 
 | 
| 
 
Upper data 
 | 
 
Data at the time of setting the event 
 | 
| 
 
Use the data mask 
 | 
 
No 
 | 
| 
 
Mask value 
 | 
 
0xFFFFFFFF 
 | 
 
Table 2.27  | Initial Values of Pass count Conditions  | 
 
| 
 
Item 
 | 
 
Initial Value 
 | 
| 
 
Pass count [Simulator] 
 | 
 
1 
 |