2.14.3  
Collect execution history in a section
 
The execution history is collected as trace data only for a section while the program is in execution by setting a Trace event.
This Trace event consists of a trace start event and a trace end event. 
To use this function, follow the procedure described below. 
 
2.14.3.1  Set a Trace event
2.14.3.2  Execute the program
2.14.3.3  Edit a Trace event
2.14.3.4  Delete a Trace event
Caution 2.  | [Simulator] 
Trace start events and trace stop events cannot be set/deleted while a tracer is running.   | 
 
Caution 3.  | [Simulator] 
If you perform a trace from a trace start event until a trace end event, the simulator will not include the trace end event in the results of the trace. For this reason, if you are using a simulator, set the trace end event one line below the range for which you require display of the trace data.  |