2.6.2.2  
Add download files (*.hex/*.mot/*.bin)
 
Follow the steps below to add download files other than the load module file format (Intel HEX file (*.hex), Motorola S-record file (*.mot), or binary file (*.bin)) in the Download Files dialog box. 
(1)  | Click the [Add] button  | 
 
When the [Add] button is clicked, a blank list item "-" is displayed in the last line of the [Download file list] area.  
(2)  | Property configuration of the download files to add   | 
 
Configure the download conditions for the download file to add in the [Download file property] area. 
Configure each item displayed with the following condition.  When the configuration is completed, the file name specified in this property is displayed in the blank list of the [Download file list] area. 
| 
 
File 
 | 
 
Specify the download file (Intel HEX file (*.hex), Motorola S-record file (*.mot), or binary file (*.bin)) to download (up to 259 characters).   
 | 
| 
 
Default 
 | 
 
Blank 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard, or specify with the Select Download File dialog box opened by clicking the [...] button. 
 | 
| 
 
Available values 
 | 
 
See "Table 2.4  Downloadable File Formats". 
 | 
| 
 
File type 
 | 
 
Select the type of the file to download.   
Here, select a item other than [Load module file]. 
 | 
| 
 
Default 
 | 
 
Load module file 
 | 
| 
 
Modifying 
 | 
 
Select from the drop-down list. 
 | 
| 
 
Available values 
 | 
 
Load module file 
 | 
 
Specifies a load module file. 
 | 
| 
 
Hex file 
 | 
 
Specifies an Intel HEX file. 
 | 
| 
 
S record file 
 | 
 
Specifies a Motorola S-record file. 
 | 
| 
 
Binary data file 
 | 
 
Specifies an binary file. 
 | 
| 
 
Offset 
 | 
 
Specify the offset from the address at which the file's download is to start.  
Note that this item appears only when [File type] is set to [Hex file] or [S record file]. 
 | 
| 
 
Default 
 | 
 
0 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard.  
 | 
| 
 
Available values 
 | 
 
0x0 to 0xFFFFFFFFFF in hexadecimal number 
 | 
| 
 
Start address 
 | 
 
Specify the address at which to start the file's download.  
Note that this item appears only when [File type] is set to [Binary file]. 
 | 
| 
 
Default 
 | 
 
0 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard.  
 | 
| 
 
Available values 
 | 
 
0x0 to 0xFFFFFFFFFF in hexadecimal number 
 | 
 
Remark  | The settings of whether to download the object information or symbol information can be made only when the type of the file to download is load module files.  | 
 
(3)  | Check the order of download   | 
 
The order of the download is the display order of the files displayed in the [Download file list] area. 
If you want to change the order, use the [Up]/[Down] button. 
Enable all the configuration in this dialog box and add a download file (the file name is displayed in the [Download] category on the [Download File Settings] tab of the Property panel).