It is possible to specify the display start position of the memory contents by specifying an address expression in the display position specification area (starting with address 0x0 by default).
An offset value of the display start position of memory values can be set via the Address Offset Settings dialog box that is opened by selecting [Address Offset Value Settings...] from the context menu.  | 
Directly enter the address expression of the memory value address to display in the text box. You can specify an input expression with up to 1024 characters. The result of the expression is treated as the display start position address.
Note that address values greater than the microcontroller address space cannot be specified.
A symbol name at the current caret position can be complemented by pressing the [Ctrl] + [Space] key in this text box (see "2.21.2 Symbol name completion function").  | 
If the specified address expression is the symbol and its size can be recognized, everything from the start address to the end address of that symbol is displayed selected.  | 
The timing to change the display start position can be determined by specifying in the [Move when Stop] check box and the [Move] button.