Everything
A.1 Description

Windows/panels/dialog boxes for debugging are listed below.

Table A.1

Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Description

Main window

Controls the program execution. Various windows, panels and dialogs can be opened from this window.

Project Tree panel

Selects the debug tool to use.

Property panel

Displays detailed information on the debug tool currently selected in the Project Tree panel, and enables the settings of the tool to be changed.

Memory panel

Displays and modifies memory values.

Disassemble panel

Displays the results of memory value disassemble and is used to execute line assemble and instruction level debug.

CPU Register panel

Displays the contents of CPU registers, and modifies register values.

SFR panel

Displays and modifies SFR values.

Local Variables panel

Displays and modifies local variables.

Watch panel

Displays and modifies registered watch-expression values.

Call Stack panel

Displays call stack information on function calls.

Trace panel

Displays trace data acquired from the debug tool.

Events panel

Displays detailed information on set events, switches the events between enabled and disabled, or deletes them.

Output panel

Displays messages output from the build tool/debug tool/plug-ins, or the results of batch searches carried out using the Find and Replace dialog box.

Memory Mapping dialog box

Sets the memory mapping.

Download Files dialog box

Selects files to be downloaded and sets the download conditions.

Action Events dialog box

Sets action events.

Security ID Input dialog box

Sets security ID.

Column Number Settings dialog box

Specifies the number of view columns of memory values on the Memory panel.

Address Offset Settings dialog box

Specifies an offset value for the address display on the Memory panel.

Memory Initialize dialog box

Initializes memory.

Memory Search dialog box

Searches memory.

Print Address Range Settings dialog box

Sets the address range to print the contents of the Disassemble panel.

Trace Search dialog box

Searches trace data.

Combination Condition dialog box [E1][E20]

Displays and modifies detailed information on a Combination Break event

Detail dialog box (for execution events)

Displays and modifies detailed information on an execution-related event.

Detail dialog box (for access events)

Displays and modifies detailed information on an access-related event.

Scroll Range Settings dialog box

Sets the scroll range for the Memory panel/Disassemble panel.

Go to the Location dialog box

Moves the caret to the specified position.

Data Save dialog box

Saves the settings and other data displayed in the respective windows/panels/dialogs or saves upload data.

Specified Section dialog box

Specifies the range for skipping step execution.

Functions and Variables Access Table panel

Displays the functions that access variables in the form of an orthogonal table.

Measuring Current Consumption panel [E2][Simulator]

This panel is central to the functionality of the solution for measuring current consumption.

Current Consumption Measurement Condition Setting dialog box [E2]

This dialog box is used to set measurement conditions in the Measuring Current Consumption panel [E2][Simulator].

Current Consumption Measurement Trigger Condition Setting dialog box [E2]

This dialog box is used to set trigger conditions in the Measuring Current Consumption panel [E2][Simulator].

Current Consumption Measurement Search dialog box [E2][Simulator]

This dialog box is used to specify and search the detailed conditions in the Measuring Current Consumption panel [E2][Simulator].

Save Current Values dialog box [E2]

This dialog box is used to save the values for current in the Measuring Current Consumption panel [E2][Simulator].

Virtual Board panel [Simulator]

This panel is used to configure the virtual target system and operate the virtual components.

 

Table A.2

Simulator GUI Block-Dedicated Window/Dialog Box List

Window/Dialog Box Name

Description

Simulator GUI window

Opens and controls various simulator GUI's windows and dialog boxes.

Customize dialog box

Setting of window colors and fonts

Signal Data Editor window

Setting of input signal data

Loop dialog box

Setting of loop information for the Signal Data Editor window

Select Pin dialog box

Selection of display pins in the Signal Data Editor window and Timing Chart window

Timing Chart window

Timing chart display of input and output signals

Search Data dialog box

Detailed search of the Timing Chart window

I/O Panel window

Creation of dummy target system

Parts Button Properties dialog box

Setting of button pin connection information

Analog Button Properties dialog box

Setting of analog button pin connection information

Parts Key Properties dialog box

Setting of key matrix LED pin information

Parts Level Gauge Properties dialog box

Setting of level gauge pin connection information

Parts Led Properties dialog box

Setting of key matrix LED pin information

Parts Segment LED Properties dialog box

Setting of 7/14-segment LED pin connection information

Parts Matrix Led Properties dialog box

Setting of matrix LED pin connection information

Parts Buzzer Properties dialog box

Setting of buzzer pin connection information

Pull up/Pull down dialog box

Setting of pull-up/pull-down resistor pin connection information

Object Properties dialog box

Setting of connection information for figure, character, and bitmap pins

Parts List dialog box

List display of object pin connection status in the I/O Panel window

Serial window

Serial interface communication window

Format (UART) dialog box

Setting of serial format (UART)

Format (CSI) dialog box

Setting of serial format (CSI)

Format (IIC) dialog box

Setting of serial format (IICA)