To reset CPU, click the
button on the debug toolbar.
When CPU is reset, the current PC value is set to the reset address.
You can automatically overwrite the value of I/O register/CPU register with the specified values after CPU reset (see "2.18 Setting Up the Hook Process" for details). |