Editing the Program
![]()

2. Editing
Edit the program following the steps listed below.
|
Double-click " r_cg_main.c " in the Project Tree. |


|
Copy the following text and paste it to the section of r_cg_main.c shown in the figure below. |
|
R_CMT0_Start(); |


|
Double-click " r_cg_cmt_user.c " in the Project Tree. |


|
Copy the following texts and paste them to the sections of r_cg_cmt_user.c shown in the figure below. |
|
uint16_t g_count; |
|
uint16_t inreg = 0,outreg = 0; g_count++; inreg = PORTA.PDR.BIT.B0; outreg = inreg ^ 1; PORTA.PDR.BIT.B0 = outreg; PORTB.PDR.BIT.B7 = inreg; |