The features of the analysis tool are shown below.
The following information about functions is displayed:
Static analysis information (e.g. function name, file name, attribute, return type, reference count, etc.) and Dynamic analysis information (e.g. execution count, execution time, code coverage, etc.).
![](Analyze_E-1.gif)
The following information about variables is displayed:
Static analysis information (e.g. variable name, file name, attribute, type, reference count, etc.) and Dynamic analysis information (e.g. read count, write count, data coverage, etc.).
![](Analyze_E-2.gif)
A tree-structured chart (call graph) indicating calling relationships between functions in the program is displayed.
![](Analyze_E-3.gif)
The class information [CC-RX], function information and variable information in the program are displayed in a tree structure.
![](Analyze_E-4.gif)
The following operations can be performed on the debug tool from the various panels of the analysis tool.
Jump to the location where the specified function or variable is defined: |
Set a break event at the specified function or variable: |
Register a watch expression for the specified variable: |
You can find and display a list of locations referencing a function/variable.
![](Analyze_E-5.gif)
A line chart indicating changes in values of variables or of data collected for Smart Analog [E1/E2/E2 Lite/E20/COM Port[RL78]] is displayed. |
![](Analyze_E-6.gif)
![](Analyze_E-7.gif)