8-bit interval timer
Below is a list of API functions output by the Code Generator for 8-bit interval timer use.
Table 3.17 API Functions: [8-Bit Interval Timer]
| API Function Name | Function | 
| Performs initialization necessary to control the 8-bit interval timer. | |
| Performs user-defined initialization relating to the 8-bit interval timer. | |
| Performs processing in response to the 8-bit interval timer interrupt INTITn0 or INTITn1. | |
| Starts the count of the 8-bit interval timer. | |
| Ends the count of the 8-bit interval timer. | |
| Halts the clock supplied to the 8-bit interval timer. | |
| Halts the clock supplied to the 8-bit interval timer. |