Performs processing in response to the CSI reception error interrupt INTSREn.
Remark This API function is called as the callback routine of interrupt process r_uartn_interrupt_error corresponding to the CSI reception error interrupt INTSREn.
[Syntax]
#include “r_cg_macrodriver.h”
static void r_csimn_callback_error ( uint8_t err_type );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint8_t err_type;  | 
    
       Trigger for CSI reception error interrupt 00000xx1B: Overrun error  | 
[Return value]
None.