Configures the operation mode of data operation circuit.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_doc.h”
MD_STATUS R_DOC_SetMode ( doc_mode_t mode, unit16_t value );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       doc_mode_t mode;  | 
    
       Operation mode of data operation circuit ADDITION : Data addition mode SUBTRACTION : Data subtraction mode COMPARE_MATCH : Data comparison mode (Detection Condition: Data match is detected) COMPARE_MISMATCH : Data subtraction mode (Detection Condition: Data mismatch is detected)  | 
| 
       I  | 
    
       uint16_t value;  | 
    
       Data addition and data subtraction : Results of operations Data comparison : 16-bit data for use as a reference  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ARGERROR  | 
    
       Invalid argument specification  |