R_KB2m_TKBOn1_SmoothStartFunction_Start
 
Starts smooth start function for timer 
output TKBOn1.
 
[Syntax]
void   
R_KB2m_TKBOn1_SmoothStartFunction_Start ( void );
 
Remark         
m is the unit number, and n is the channel number.
 
[Argument(s)]
None.
 
[Return 
value]
None.