Reads the results of A/D conversion.
[Syntax]
#include “r_cg_macrodriver.h”
void R_PGA_DSAD_Get_Result ( uint16_t * const bufferH, uint16_t * const bufferL );
[Argument(s)]
| I/O | Argument | Description | 
| O | uint16_t * const bufferH; | Pointer to area in which to store the results of A/D conversion (DSADCRM resister and DSADCRH resister) | 
| O | uint16_t * const bufferLl; | Pointer to area in which to store the results of A/D conversion (DSADCRC resister and DSADCRL resister) | 
[Return value]
None.