Reads the pulse width of the 16-bit timer RDn.
Remark 1. This API function can only be called when the 16-bit timer RDn is being used for input capture function.
Remark 2. If there is an overflow (2 pulses or more) during pulse-width measurement, then the pulse width will not be read correctly.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_timer.h”
MD_STATUS  
R_TMRDn_Get_PulseWidth ( uint32_t * const 
active_width,
uint32_t * const inactive_width, timer_channel_t 
channel );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       unit32_t * const active_width;  | 
    
       Pointer to an area storing the active level width that was read  | 
| 
       O  | 
    
       uint32_t * const inactive_width;  | 
    
       Pointer to an area storing the inactive level width that was read  | 
| 
       I  | 
    
       timer_channel_t channel;  | 
    
       in to read TMCHANNELA : TRDIOAn pin TMCHANNELB : TRDIOBn pin TMCHANNELC : TRDIOCn pin TMCHANNELD : TRDIODn pin  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  |