Usage example
Use Operational amplifer for Comparator as + side input.
[GUI setting example]
| 
       Operational amplifer  | 
    ||||
| 
       OPAMP  | 
    
       Used  | |||
| 
       Operational amplifer operation setting  | 
    
       Used  | |||
| 
       Use operational amplifer 0  | 
    
       Used  | |||
| 
       Use operational amplifer 1  | 
    
       Unused  | |||
| 
       Use operational amplifer 2  | 
    
       Unused  | |||
| 
       Use operational amplifer 3  | 
    
       Unused  | |||
| 
       Reference current circuit setting  | 
    
       Stop  | |||
| 
       
  | 
    
       
  | 
    
       
  | 
    
       Operation mode setting  | 
    
       Low-power mode  | 
| 
       
  | 
    
       
  | 
    
       
  | 
    
       ELC trigger setting  | 
    
       Operational amplifer 0: Opeartional amplifer ELC trigger 0  | 
| 
       Operational amplifer 1: Opeartional amplifer ELC trigger 1  | ||||
| 
       Operational amplifer 2: Opeartional amplifer ELC trigger 2  | ||||
| 
       Operational amplifer 3: Opeartional amplifer ELC trigger 3  | ||||
| 
       
  | 
    
       
  | 
    
       Operational Amplifier 0  | 
    
       Used  | |
| 
       
  | 
    
       
  | 
    
       
  | 
    
       Activation/stop trigger control setting  | 
    
       Software trigger mode  | 
| 
       Comparator  | 
    ||||
| 
       COMP  | 
    
       Used  | |||
| 
       Operation setting  | 
    
       Use only comparator 0 (Comparator input:AMP0O)  | |||
| 
       Speed setting  | 
    
       Low speed  | |||
| 
       Comparator 0  | 
    
       Used  | |||
| 
       Comparator0 Mode setting  | 
    
       Normal  | |||
| 
       Comparator0 Edge setting  | 
    
       Rising edge  | |||
| 
       Comparator0 Digital filter setting  | 
    
       Unused  | |||
| 
       
  | 
    
       
  | 
    
       
  | 
    
       Comparator0 Enable output (VCOUT0)  | 
    
       Unused  | 
| 
       
  | 
    
       
  | 
    
       
  | 
    
       Comparator0 Use comparator 0 interrupt (INTCMP0)  | 
    
       Used  | 
| 
       
  | 
    
       
  | 
    
       
  | 
    
       Comparator0 Priority  | 
    
       Low  | 
[API setting example]
r_cg_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start the operational amplifier 0 */
R_OPAMP0_Start();
/* Start the comparator 0 */
R_COMP0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}