-
vrst_dtq
-
ER vrst_dtq (ID dtqid);
|
|
|
|
|
|
ID dtqid;
|
ID number of the data queue.
|
This service call reset the data queue specified by parameter
dtqid.
The data having been accumulated by the data queue area are annulled. The tasks to wait to send data to the target data queue are released from the WAITING state, and EV_RST is returned as a return value for the tasks.
Note 1 In this service call, the tasks to wait to receive data do not released from the WAITING state.
Note 2 This service call is the function outside
mITRON4.0 specification.
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
|
|
|
|
- Stack pointer points out of user stack for invoking task.
|
|
|
|
- The data queue specified by dtqid does not exist.
|