< Compile Options / List Options >
[Format]
-show=<sub>[,...]
<sub>: { source | conditionals | definitions | expansions }
|
[Description]
- | This option sets the source list file contents. |
- | The suboptions and specified contents are shown in the following table. |
Table 2.5 | Suboption Specifications |
|
|
|
|
source
|
Outputs the C/C++ source file.
|
|
conditionals
|
Outputs also the statements for which the specified condition is not satisfied in conditional assembly.
|
|
definitions
|
Outputs the information before .DEFINE replacement.
|
|
expansions
|
Outputs the assembler macro expansion statements.
|
[Remarks]
- | This option is valid only when the listfile option has been specified. |
- | Information output from the compiler is written to the source list. For the source list file format, refer to Assemble List File. |