5.2.6
Specific Compiler Directives
The following directives are output in some cases so that the assembler can appropriately process C language functions when the compiler generates assembly-language files.
When using the assembly-language files generated by the compiler, these directives should be used without changing the settings. These directives should not be used when creating user-created assembly-language files.
Table 5.31 | Specific Compiler Directives |
|
|
|
|
._LINE_TOP
|
These directives are output when the functions specified by #pragma inline_asm have been expanded.
|
|
._LINE_END
|
|
.SWSECTION
|
These directives are output when the branch table is used in the switch statement.
|
|
.SWMOV
|
|
.SWITCH
|
|
.INSTALIGN
|
This directive is output when the instalign4 option, the instalign8 option, #pragma instalign4, or #pragma instalign8 is used.
|