This dialog box is used to set the debugging.
![](RH850_Debug_E-689.gif)
The following items are explained here.
On the [Connect Settings] tab of the Property panel, click the [...] button displayed by selecting one of the values of the [Debug target] property in the [Multi-core] category. |
This area displays a list of contexts for debugging.
When a checkbox is selected, the selected context is handled as a target for debugging.