Everything

[State save event] tab


This tab is used to configure how to save and restore the state of the debug tool upon occurrence of an action event.

Note that the data to be restored is limited to memory and register values that can be read or written.

Figure A.33

Action Events Dialog Box: [State save event] Tab

 

This section describes the following.

[How to open]

-

On the Editor panel, move the caret to the line where you wish to set a State save event, then select [Register Action Event...] from the context menu.

-

On the Disassemble panel, move the caret to the address where you wish to set a State save event, then select [Register Action Event...] from the context menu.

-

On the Events panel, select a State save event, then select [Edit Condition...] from the context menu.

[Description of each area]

(1)

[Save debug tool state n] area

When an action event occurs, the state of the debug tool is saved in a file as the n-th data.

(2)

[Restore debug tool state n] area

When an action event occurs, the state of the debug tool is restored from the n-th data file.

(3)

[Address] area

Specify the address at which to set a state save event.

You can either type an address expression directly into the text box (up to 1024 characters), or select them from the input history via the drop-down list (up to 10 items). The address of the location currently being specified is displayed by default.