Configure the operating environment on the Property panel below when using E1.
Note that the contents of the Property panel differ depending on the communication method (FINE communications [E1(Serial)] or JTAG communications [E1(JTAG)]) between E1 and the target system.
![](Debug_RX_E-33.gif)
![](Debug_RX_E-34.gif)
Follow the steps below by selecting the corresponding tab on the Property panel.
2.3.2.1 [Connect Settings] tab
2.3.2.2 [Debug Tool Settings] tab