When deleting a break event (access-related) you have set, first open the Events panel by selecting [View] menu >> [Event], and then perform the following operations. Note that event name differs depending on the debug tool to use.
After selecting the break event (access-related) you wish to delete in the detailed information on the combination break, click (
) button on the toolbar in the above panel (see “2.17.5 Deleting events“).
Each break event (access-related) can also be deleted by clicking on the event mark on the disassembled text.
After selecting the hardware break (access-related) you wish to delete, click (
) button on the toolbar in the above panel (see “2.17.5 Deleting events“).